Start
> notebooks/laptops
> Acer LX.E970X.023
|
 |
Extensa 5620Z-2A2G12Mi |
|
Brand: Acer
Product code: LX.E970X.023
EAN/UPC code: 0099802464004
|
Category: notebooks/laptops
|
|
|
|
|
Release date: 05 May 2008
Info modified on: 03 Dec 2008 23:30:09
Intel® Pentium® Dual-Core processor T2330 (1.46GHz/FSB: 533MHz/1MB L2 cache), Microsoft® Windows® Vist™ Home Premium, Microsoft® Office Ready 2007 (trial version), 15.4" TFT WXGA CrystalBrite, 2GB DDR II RAM (2x 1GB), 120GB HDD (5400rpm), Super Multi DVD-RW Double Layer, 6-cell Li-ion, 56K modem, Gigabit & Wireless LAN 802.11b/g, Mobile Intel® Graphics Media Accelerator X3100 128MB shared, no cam
|
|
|
|
|
|
A notebook, also known as laptop, is a portable computer. When you are looking for the right notebook, it is important to know where you are going to work with it. Do you want to use it on the road? Choose a model with a special energy saving 'mobile' processor, a good battery and a reasonably small display. This will allow you to work longer with the same battery and saves you the trouble of carrying around a large display that consumes a lot of precious battery power. Or will you be using you notebook mainly in places where you will have access to a power outlet? Then choose a desktop processor (more processing power for less money) and an ordinary battery, this will save you a lot of money, which you could spend on a bigger screen, you'll work faster because you can view more information at once and it's great for multimedia!
|
 |
 |
 |
|
|
The new Acer Extensa 5620Z is designed for the business professionals looking for the perfect balance between performance and affordable mobile technology. Equipped with the cutting edge Intel® Pentium® dual-core mobile processor and featuring a 15.4” widescreen display with optional integrated CrystaEye video camera, the new Extensa 5620Z is the perfect example of Acer’s strategy to provide powerful tools for your daily business.
|
|
 |
Specs
|
Alternatives
|
Options
|
|
|
|
Processor clock speed
|
|
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1460 MHz
|
|
Processor family
|
|
The processor serie to which the processor belongs.
Intel Pentium Dual-Core
|
|
Processor
|
|
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
Intel Pentium Dual Core T2330
|
|
Processor front side bus
|
|
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
533 MHz
|
|
L2 cache
|
|
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
1 MB
|
|
Hard disk drive capacity
|
|
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
120 GB
|
| Hard disk interface |
SATA |
|
Hard disk rotational speed
|
|
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
|
|
Display diagonal
|
|
Size of the display for this product; expressed in inches diagonal
15.4 "
|
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
WXGA TFT LCD
|
|
Display resolution
|
|
Resolution of the display for the system
1280 x 800 pixels
|
|
Number of colours
|
|
Maximum number of viewable colors.
16.7 M
|
|
Internal memory
|
|
The amount of memory measured in megabytes installed in the system's hardware
2048 MB
|
| Internal memory type |
DDR2 SDRAM |
|
Memory layout
|
|
Describe how memory is plugged on the motherboard
2 x 1024 MB
|
| Compatible memory cards |
SD/MMC/MS/MS Pro/xD |
| Graphic adapter |
Intel GMA X3100 |
|
Maximum graphic adapter memory
|
|
Graphics memory is determining with the (graphic) processor, the graphics/video performance of your computer. Graphics memory is often shared with system memory so that it varies depending on the amount of system memory installed and system load.
128 MB
|
|
Optical drive type
|
|
Type of the optical drive
DVD±RW DL
|
| Built-in microphone |
 |
| Audio system |
High Definition Audio |
| Number of built-in speakers |
2 |
| Keyboard function keys |
12 |
| Keyboard number of keys |
88 / 89 |
| Camera included |
 |
| Internal modem |
 |
| Networking features |
Gigabit Ethernet |
| Wake-on-Ring ready |
 |
| Wireless technology |
IEEE 802.11b/g |
| Modem speed |
56 Kbit/s |
| Wake-on-LAN ready |
 |
|
Bluetooth
|
|
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
|
|
|
|
|
|
|
| components |
 |
|
NS-LC100 |
NOTEBOOK KOELER NEWSTAR LC-100 |
|
| hard disk drives |
 |
 |
SPE3030CC/00 |
External Hard Disk, 320GB |
|
 |
 |
Case-USB218-60 |
HT-18A |
|
 |
 |
CASE-USB218-20BL |
HT-18A |
|
 |
 |
Case-USB218-40BL |
HT-18A |
|
| Show all hard disk drives >> | | keyboards & desktops |
 |
 |
313518 |
Wireless Keyboard & Mouse Belinea o.board US White |
|
 |
 |
KP002 |
Portable USB Keypad and 2 Port HUB |
|
| network cards & adapters |
 |
 |
DWA-140 |
Wireless N USB Adapter |
|
 |
 |
20002325 |
FRITZ!WLAN USB Stick |
|
 |
 |
3CRUSB10075 |
OfficeConnect Wireless 54Mbps 11g Compact USB Adapter |
|
 |
 |
20002420 |
FRITZ!WLAN USB Stick N |
|
 |
 |
CN-WF518D |
Network Adapter, Wireless, 54Mbps, Retail, IEEE 802.11b/IEEE 802.11g, USB 2.0 |
|
 |
 |
DWA-645 |
RangeBooster N650 Draft-11n PC Card |
|
 |
 |
Z 14438 Z |
Link Z 14438 Z |
|
| Show all network cards & adapters >> | | flash memory |
 |
 |
SI-707134 |
Flash Drive With Encryption Software 8GB |
|
| antivirus & security software |
 |
 |
2869 |
AntiVirus 2008 NL |
|
 |
 |
2870 |
InternetSecurity 2008 NL |
|
 |
 |
2867 |
TotalCare 2008 NL |
|
 |
 |
11057341 |
Norton 360 (NL) WinXP/Vista |
|
 |
 |
Q12P08 |
Internet Security 2008, 3-user, 1 Year, NL |
|
 |
 |
Q12T08 |
Antivirus + Firewall 2008, 3-user, 1 Year, NL |
|
 |
 |
KL1125NLBOX |
Kaspersky® Anti-Virus 7.0, CROM, Box, NL |
|
 |
 |
KL1825NLBOX |
Kaspersky® Internet Security 7.0, CDROM, Box, NL |
|
 |
 |
Q12L08 |
Antivirus 2008, 3-user, 1 Year, NL |
|
 |
 |
ETRAV8001BPEM |
eTrust Avirus r8 NON CD W32 1user |
|
 |
 |
ETRITM8001BPEM |
Integrated Threat Management r8 in English - 1 User - Product only - 1 Year |
|
 |
 |
ETRPPCE8001BPEM |
eTrust PestPatrol Corporate Edition r 8in English French Italian German Spanish and Japanese - 1 User - Product only |
|
| Show all antivirus & security software >> | | mice |
 |
 |
CLLMTRAVEL |
Lounge’n’LOOK Travel Mouse |
|
 |
 |
MICROII-EU |
USB optical micro mouse |
|
 |
 |
931669-0914 |
V450 Laser Cordless Mouse for Notebooks |
|
 |
 |
MI015 |
Mini Wireless Optical Mouse |
|
 |
 |
AI-707911 |
Wireless Optical Notebook Mouse |
| | | | |