Start
> notebooks/laptops
> Acer LX.E870Y.051
|
 |
Extensa 5220-051G08Mi |
|
Brand: Acer
Product code: LX.E870Y.051
EAN/UPC code: 0099802220723
|
Category: notebooks/laptops
|
|
|
|
|
Intel® Celeron® M processor 530, Microsoft® Windows® Vista™ Home Basic, 15.4TFT WXGA CrystalBrite, 1024MB DDR II RAM (1x 1024), 80GB HDD (5400rpm), Super Multi DVD-RW Double Layer, 6-cell LiIon, 56K modem, Gigabit & Wireless LAN 802.11b/g, 128MB shared video, S-video, FIR, 5-in-1 card reader
|
|
|
|
|
|
A notebook, also known as laptop, is a portable computer. When you are looking for the right notebook, it is important to know where you are going to work with it. Do you want to use it on the road? Choose a model with a special energy saving 'mobile' processor, a good battery and a reasonably small display. This will allow you to work longer with the same battery and saves you the trouble of carrying around a large display that consumes a lot of precious battery power. Or will you be using you notebook mainly in places where you will have access to a power outlet? Then choose a desktop processor (more processing power for less money) and an ordinary battery, this will save you a lot of money, which you could spend on a bigger screen, you'll work faster because you can view more information at once and it's great for multimedia!
|
 |
 |
 |
|
|
The new Acer's Extensa 5220 features the new ProFile design chassis and is empowered by the latest Intel® Celeron® Mobile processors. Featuring a comprehensive and outstanding 15.4" widescreen in combination with the optional Acer CrystalEye video camera, the latest graphics and full wireless communication, the Extensa 5220 is enhancing your efficiency in any mobile business environment.
|
|
 |
Specs
|
Alternatives
|
Options
|
|
|
|
Processor clock speed
|
|
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1730 MHz
|
|
Processor family
|
|
The processor serie to which the processor belongs.
Intel Celeron M
|
|
Processor
|
|
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
Intel Celeron M 530
|
|
Processor front side bus
|
|
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
533 MHz
|
|
Chipset
|
|
Chipset for this configuration; expressed as manufacturer and coined name
Mobile Intel GL960 Express
|
|
L2 cache
|
|
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
1 MB
|
|
Hard disk drive capacity
|
|
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).
80 GB
|
| Hard disk interface |
SATA |
|
Hard disk rotational speed
|
|
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
|
|
Display diagonal
|
|
Size of the display for this product; expressed in inches diagonal
15.4
|
|
Display
|
|
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend.
In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
WXGA TFT LCD
|
|
Display resolution
|
|
Resolution of the display for the system
1280 x 800 pixels
|
|
Number of colours
|
|
Maximum number of viewable colors.
16.7 M
|
|
Internal memory
|
|
The amount of memory measured in megabytes installed in the system's hardware
1024 MB
|
|
Memory slots
|
|
Number and type of memory expansion slots; including connector and memory module descriptions
so-DIMM
|
| Internal memory type |
DDR2 SDRAM |
|
Memory layout
|
|
Describe how memory is plugged on the motherboard
1 x 1024 MB
|
| Maximum internal memory |
2 GB |
| Compatible memory cards |
SD/MMC/MS/MS Pro/xD |
| Graphic adapter |
Intel GMA X3100 |
|
Maximum graphic adapter memory
|
|
Graphics memory is determining with the (graphic) processor, the graphics/video performance of your computer. Graphics memory is often shared with system memory so that it varies depending on the amount of system memory installed and system load.
128 MB
|
|
Optical drive type
|
|
Type of the optical drive
DVD±RW DL
|
| Built-in microphone |
 |
| Audio system |
High Definition Audio |
| Number of built-in speakers |
2 |
| Keyboard function keys |
12 |
| Keyboard number of keys |
88 / 89 |
| Camera included |
 |
| Internal modem |
 |
| Networking features |
Gigabit Ethernet |
| Wake-on-Ring ready |
 |
| Wireless technology |
IEEE 802.11b/g |
| Modem speed |
56 Kbit/s |
| Modem type |
ITU V.92 |
| Wake-on-LAN ready |
 |
|
|
Bluetooth
|
|
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
|
| Wireless LAN data transfer rate (max) |
54 Mbit/s |
| Operating system provided |
Windows Vista Home Basic Edition |
| Battery technology |
Lithium-Ion |
|
Battery life
|
|
Maximum battery life in hours. Mobile Mark™ (2002) is the standard often used to benchmark battery life time. In some cases battery life can be extended by adding extra batteries.
2.5 h
|
| Number of battery cells |
6 |
| ExpressCard slot |
 |
| VGA (D-Sub) ports quantity |
1 |
| Ethernet LAN (RJ-45) ports quantity |
1 |
| IEEE 1394/Firewire ports quantity |
1 |
|
TV out port
|
|
Description of TV Out port
S-Video
|
|
USB 2.0 ports quantity
|
|
USB 2.0 ports have a data transmission speed of 480 Mbps, and are backwards compatible with USB 1.1 ports. You can connect all kinds of peripheral devices to them.
4
|
| Modem (RJ-11) ports |
1 |
| Speaker/ headphone/ line-out jack |
1 |
| Microphone, line-in jack |
 |
| S/PDIF out port |
 |
| DC-in jack |
 |
| DVI port |
 |
|
Infrared data port
|
|
A data port that uses infra-red data association (irDA) as the standard for wireless communications between computer and mobile phone devices. For example, to update the phone list on your irDA-enabled PC, you would line up the infra-red ports on each device and then transfer the phone information to your PC. This is a wireless transfer, so you don't need a cable or extra software.
|
| CardBus PCMCIA slots quantity |
1 |
| SmartCard slot |
 |
| CardBus PCMCIA slot type |
Type II |
| TV in port |
 |
| Port replicator |
 |
| Cable lock slot |
Kensington |
| BIOS password |
 |
|
Weight
|
|
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.
2880 g
|
|
Dimensions W x D x H
|
|
Dimensions of the produkt (Width x Depth x Height) in millimeter.
360 x 267 x 43 mm
|
| Depth |
267 mm |
|
Height
|
|
Height of the product
43 mm
|
| Width |
360 mm |
| Pointing device |
Touchpad |
|
|
|
|
|
| hard disk drives |
 |
 |
CASE-USB218-20BL |
HT-18A |
|
 |
 |
Case-USB218-60 |
HT-18A |
|
 |
 |
Case-USB218-40BL |
HT-18A |
|
 |
 |
SPE3030CC/00 |
External Hard Disk, 320GB |
|
| Show all hard disk drives >> | | keyboards & desktops |
 |
 |
313518 |
Wireless Keyboard & Mouse Belinea o.board US White |
|
 |
 |
KP002 |
Portable USB Keypad and 2 Port HUB |
|
| network cards & adapters |
 |
 |
DWA-140 |
Wireless N USB Adapter |
|
 |
 |
20002325 |
FRITZ!WLAN USB Stick |
|
 |
 |
3CRUSB10075 |
OfficeConnect Wireless 54Mbps 11g Compact USB Adapter |
|
 |
 |
20002420 |
FRITZ!WLAN USB Stick N |
|
 |
 |
CN-WF518D |
Network Adapter, Wireless, 54Mbps, Retail, IEEE 802.11b/IEEE 802.11g, USB 2.0 |
|
 |
 |
Z 14438 Z |
Link Z 14438 Z |
|
 |
 |
DWA-645 |
RangeBooster N650 Draft-11n PC Card |
|
| Show all network cards & adapters >> | | flash memory |
 |
 |
SI-707134 |
Flash Drive With Encryption Software 8GB |
|
| mice |
 |
 |
CLLMTRAVEL |
Lounge’n’LOOK Travel Mouse |
|
 |
 |
MICROII-EU |
USB optical micro mouse |
|
 |
 |
MI015 |
Mini Wireless Optical Mouse |
|
 |
 |
931669-0914 |
V450 Laser Cordless Mouse for Notebooks |
|
 |
 |
AI-707911 |
Wireless Optical Notebook Mouse |
|
| Show all mice >> | | notebook bags & cases |
 |
 |
CN31 |
Notebook Case |
|
 |
 |
CN01 |
Notepac |
|
 |
 |
NCV1 |
Basic Laptop Case 15.4" |
|
 |
 |
PX1411E-1NCA |
Carry Case Value Edition 15.4" |
|
 |
 |
PX1419E-1NCA |
EasyGuard Business Carry Case 17" |
|
 |
 |
PNC15 |
15.4" Slimline Laptop Case |
|
 |
 |
KLC15 |
15.4" Lightweight Professional Laptop Case |
|
 |
 |
N 16358 N |
VisionPlus 15/15.4" |
|
 |
 |
N 11018 A |
AluSlight |
|
| Show all notebook bags & cases >> | | antivirus & security software |
 |
 |
2869 |
AntiVirus 2008 NL |
|
 |
 |
2867 |
TotalCare 2008 NL |
|
 |
 |
2870 |
InternetSecurity 2008 NL |
|
 |
 |
Q12T08 |
Antivirus + Firewall 2008, 3-user, 1 Year, NL |
|
 |
 |
Q12P08 |
Internet Security 2008, 3-user, 1 Year, NL |
|
 |
 |
Q12L08 |
Antivirus 2008, 3-user, 1 Year, NL |
|
 |
 |
KL1125NLBOX |
Kaspersky® Anti-Virus 7.0, CROM, Box, NL |
|
 |
 |
11057341 |
Norton 360 (NL) WinXP/Vista |
|
 |
| | | | |