IceCat.biz cool in catalogues.
Search
 Netherlands Germany Spain United States Belgium Italy France Denmark UnitedKingdom Sweden Finland Austria Switzerland China Ukraine India Russian Federation Georgia Poland Portugal  More >> Country Language: English

Start > notebooks/laptops > Acer LX.AK60X.034

Aspire 7520G-302G16Mi

Brand: Acer
Product code: LX.AK60X.034
EAN/UPC code: 4718235325541
Product family: Aspire 7520
Category: notebooks/laptops 
A notebook, also known as laptop, is a portable computer. When you are looking for the right notebook, it is important to know where you are going to work with it. Do you want to use it on the road? Choose a model with a special energy saving 'mobile' processor, a good battery and a reasonably small display. This will allow you to work longer with the same battery and saves you the trouble of carrying around a large display that consumes a lot of precious battery power. Or will you be using you notebook mainly in places where you will have access to a power outlet? Then choose a desktop processor (more processing power for less money) and an ordinary battery, this will save you a lot of money, which you could spend on a bigger screen, you'll work faster because you can view more information at once and it's great for multimedia!
Release date: 13 Jul 2007
Info modified on: 30 Jun 2009 11:20:03
Aspire 7520G-302G16Mi, AMD Mobile Turion™ 64 X2 Dual-Core processor TL56 (1.8GHz), Microsoft® Windows® Vista™ Home Premium, Works 8.5 + Office Home & Student 2007 Trial (60 days), 17TFT WXGA+ CrystalBrite, 2048MB DDR II RAM (2x 1024), 160GB HDD (5400rpm), Super Multi DVD-RW Double Layer, 6-cell LiIon, 56K modem, Gigabit & Wireless Lan 802.11b/g, Up to 896MB NVIDIA® GeForce® 8400M GS TurboCache (256MB dedicated), 5-in-1 card reader, 0.3MP CrystalEye
LX.AK60X.034 Acer
43k

186k
134k
130k

The Acer TravelMate 7520 has everything companies need to maximize their business performance. Boasting a superb 17” widescreen TFT panel and equipped with the powerful AMD Turion™ 64 X2 Mobile Technology it provides a complete solution for today’s demanding business users at great value. The 17” wide TFT panel with optional integrated Acer CrystalEye webcam, up to two large serial-ATA hard ... More>>>

Specs
Alternatives
Options
Processor
Processor clock speed
Processor speed in Mhz. Often the clock speed is expressed by a manufacturer in GHz (1 GHz = 1000 MHz). The clock rate is the fundamental rate in cycles per second (measured in hertz) at which a computer performs its most basic operations such as adding two numbers. There are more factors, like internal memory size, that influence a computer's actual response time.
1800 MHz
Processor family
The processor serie to which the processor belongs.
AMD Turion 64 X2 Mobile
Processor
Processor is the central unit in a computer containing the logic circuitry that performs the instructions of a computer's programs.
Turion 64 X2 TL-56
Processor front side bus
Speed of the processor's Front Side Bus (FSB) in megahertz (1 million Herz). The FSB is the bus that transfers data between the CPU and the northbridge of the Motherboard. The maximum theoretical bandwidth of the FSB is determined by the product of its width, its clock frequency and the number of data transfers it performs per clock tick.
800 MHz
L2 cache
The CPU cache (Level 2 in megabyte) is a smaller, faster memory which stores copies of the data from the most frequently used main memory locations.
1 MB
Disk drive
Total storage capacity
Total storage capacity in Gigabyte (1 billion bytes).
160 GB
Hard disk rotational speed
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
5400 RPM
Display
Display diagonal
Size of the display for this product; expressed in inches diagonal
17 "
Display
The display technology. Flat screen technologies like Liquid Cristal Display (LCD) and Thin Film Transistor (TFT) active matrix technology are the trend. In TV technologies one can notice FST (Flat Screen Tube) technology, and ARASC (Anti Reflexion, Anti Static Coating) or AGARAS (Anti-Glare ARASC) or simply AGC (anti-glare coating). The old tv and screen technology CRT means Cathodic Ray Tube. MLA = Micro Lens Array. p-Si=Polycrystalline Silicon. a-Si=Amorphous Silicon.
TFT 17" WXGA+
Display resolution
Resolution of the display for the system
1440 x 900 pixels
Memory
Internal memory
The amount of memory measured in megabytes installed in the system's hardware
2048 MB
Internal memory type DDR2
Memory layout
Describe how memory is plugged on the motherboard
2 x 1024 MB
Maximum internal memory 4 GB
Memory clock speed 533/667 MHz
Storage media
Compatible memory cards SD, MMC, MemoryStick, Memory Stick Pro, xD Card
Card reader integrated
Video
Graphic adapter NVIDIA GeForce Go 8400M GS 896 Mb TC
Maximum graphic adapter memory
Graphics memory is determining with the (graphic) processor, the graphics/video performance of your computer. Graphics memory is often shared with system memory so that it varies depending on the amount of system memory installed and system load.
896 MB
Optical drive
Optical drive type
Type of the optical drive
DVDRW (R DL) / DVD-RAM
CD write speed 24 x
CD read speed 24 x
CD rewrite speed 16 x
DVD-RAM write speed 5 x
DVD-RW read speed 6 x
DVD+RW write speed 8 x
DVD read speed 8 x
DVD write speed 8 x
Camera
Camera included
Megapixel
MegaPixels: The number (in millions) of light-sensitive picture elements, or pixels, actually used by the camera's image sensor (CCD) to record light, and which are reflected to the final number of recorded pixels stored on the memory card.
0.3 MP
Networking
Internal modem
Bluetooth
Bluetooth is a low-power radio technology developed to replace the cables and wires currently used to link or connect electronic devices such as personal computers, printers, and a wide variety of handheld devices including mobile phones. Because it uses radio-wave connectivity, a Bluetooth-enabled device has a constant, established connection to whatever browser it uses. This saves the user the trouble of logging on to check for emails or news updates, for example.
Wireless technology Ethernet, Fast Ethernet, Gigabit Ethernet, IEEE 802.11b, IEEE 802.11g
Networking
Modem speed 56 Kbit/s
Modem type V.92
Operating system/software
Operating system provided Windows Vista Home Premium Edition
Energy management
Battery technology Lithium-Ion
Battery life
Maximum battery life in hours. Mobile Mark™ (2002) is the standard often used to benchmark battery life time. In some cases battery life can be extended by adding extra batteries.
2.5 h
Number of battery cells 6 pcs
External power adapter
Connectivity
ExpressCard slot
VGA (D-Sub) ports quantity 1
Ethernet LAN (RJ-45) ports quantity 1
TV out port
Description of TV Out port
S-Video
USB 2.0 ports quantity
USB 2.0 ports have a data transmission speed of 480 Mbps, and are backwards compatible with USB 1.1 ports. You can connect all kinds of peripheral devices to them.
4
Modem (RJ-11) ports 1
Speaker/ headphone/ line-out jack
Microphone, line-in jack
S/PDIF out port
DC-in jack
DVI port
Infrared data port
A data port that uses infra-red data association (irDA) as the standard for wireless communications between computer and mobile phone devices. For example, to update the phone list on your irDA-enabled PC, you would line up the infra-red ports on each device and then transfer the phone information to your PC. This is a wireless transfer, so you don't need a cable or extra software.
CardBus PCMCIA slots quantity 1
SmartCard slot
CardBus PCMCIA slot type Type II
TV in port
Port replicator
Weight & dimensions
Weight
Weight of the product without packaging (nett weight). If possible, the nett weight is given including standard accessories and supplies. Please, note that sometimes the manufacturer is giving a too commercial interpretation of product weight, by leaving out the weight of accessories and/or supplies.
3700 g
Dimensions W x D x H
Dimensions of the produkt (Width x Depth x Height) in millimeter.
400 x 295 x 43 mm
Depth 295 mm
Height
Height of the product
43 mm
Width 400 mm
Technical details
Pointing device Touchpad